SPWF04SA - UART_IRQHandler issue
- January 14, 2019
- 2 replies
- 1685 views
Hello,
I am developing a program with a WiFi socket user interface. I can communicate with the module using the Socket Test App. I give a certain command and my MCU does something. I generally found this to work fine until it came back after running certain functions. Initially it seemed to me like the UART interrupt just kept firing over and over again, and wouldn't continue as it should, so I stopped it running any functions after receiving commands, but it still occurs.
I now realize that what is really happening is the HAL_UART_IRQHandler isn't acting like it does earlier in the program. When the client sends it data, the callback function echos it back to the client. When this happens the program hits the break point shown in the screenshot (UART_EndTransmit_IT). However when the program fails it is because it doesn't reach this breakpoint.
So my question is about the flags the if statement above references, USART_CR1_TCIE and USART_SR_TC.
if(((isrflags & USART_SR_TC) != RESET) && ((cr1its & USART_CR1_TCIE) != RESET))
What does this line actually mean?
Do the two interrupt flags change from hardware, or are they changed in code somewhere?
And of course, any thoughts on how I can fix this issue?
Thanks