“ST-Link Debugging Issue: Launch Debugging Failed on STM32 Blue Pill”
Hello Everyone,
I am attempting to debug code on the STM32 Blue Pill board. The project compiles successfully, but when I start a debug session, it fails with the message “Launch debugging failed,” along with additional error details shown below. I would appreciate any guidance on resolving this issue.
Note: I am using an ST-Link V2 programmer (A2020 version).
Wiring is done correctly checked multiple time.
I had doubts about the Debugger configurations. Are there any other settings must be modifiable, or any other ways are
there?
" Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (18) Could not verify ST device! Abort connection."