Skip to main content
Oleksandr Yaremchuk
Associate
November 6, 2017
Question

STHV800 rx amplitude problem

  • November 6, 2017
  • 0 replies
  • 1116 views
Posted on November 06, 2017 at 13:47

Hello Communnity

I use the eval board STEVAL-IME013V1

Input frequency 40kHz

Transmission of a sin 40kHz signal from XDCR8 to LVOUT8 1:1

When the piezoelectric element UTR-1440K is switched on to the XDCR8 connector, the level of the received signal ~ 5mV

When the UTR-1440K piezoelectric element is switched off from the XDCR8 connector, the level of the received 30mV

When the piezoelectric element MA40E8 is switched on to the XDCR8 connector, the level of the received signal ~ 10mV

When the MA40E8 piezoelectric cell is switched off from the XDCR8 connector, the level of the received signal 70 mV

Question: why the large attenuation of the received signal with switched on piezoelement?

Piezoelement switched on directly to smb 

All datasets and oscillograms in the attachment
This topic has been closed for replies.