STM32F103C8T6 Bluepill Issue with CubeIDE
Hi Team,
I was working on STM32F103C8T6 Bluepill board. I was using this board with ST-LinkV2 to connect with CubeIDE. When i tried to flash a sample LED blink program via CubeIDE, it gave an error saying 'Target not found'. But at the same time i was able to connect this board via cube programmer using same ST-Link and write sample LED code into the board.
I have also tried to put the board into DFU mode by changing BOOT0 to 1 and connected with a usb cable to my linux machine. when i tried 'lsusb' it didnt show DFU mode status of the board. Please help me to resolve this issue.