Skip to main content
Associate III
May 13, 2025
Solved

STM32H753ZI SPI SD Card Not Responding to CMD0/CMD8 (0xFF Response)

  • May 13, 2025
  • 1 reply
  • 497 views

Hi everyone,

I’m working with an STM32H753ZI and trying to interface a 32GB SDHC card via SPI using FatFs.
The SPI connection seems fine (I can read 0xFF repeatedly), but the SD card does not respond to CMD0 or CMD8 — both return 0xFF. As a result, f_mount fails with error code (3).

Test setup:

  • STM32H753ZI

  • SPI1 @ 256 prescaler

  • 3.3V SD Card Module (Pzsmocn PZSSD001)

  • Netac 32GB SDHC card (format is FAT32 )

Observed:

  • SPI lines work (0xFF received repeatedly).

  • CMD0 and CMD8 always return 0xFF.

  • Tried keeping CS low, delaying, reformatting — no change.

Questions:

  1. Is 32GB SDHC over SPI known to have compatibility issues on STM32H753ZI?

  2. Any proven SD cards or modules you recommend?

  3. Any other suggestions to debug this issue?

HANITALY_0-1747123903799.png

 

Thank you for any help or advice!

Best answer by Mike_ST

Hello,

>> Is 32GB SDHC over SPI known to have compatibility issues on STM32H753ZI?

No

>> Any other suggestions to debug this issue?

Check the SPI bus with a scope to see what is happening.

 

You have an "SDCARD over SPI" example in the STM32H7 software package:

STM32H7 software package 

under:

Projects\NUCLEO-H743ZI\Applications\FatFS\FatFS_uSD_Standalone

It should be compatible with H753.

Perhhaps you'll have to change the SPI instance and the SPI pins.

 

1 reply

Mike_ST
Mike_STBest answer
Technical Moderator
May 13, 2025

Hello,

>> Is 32GB SDHC over SPI known to have compatibility issues on STM32H753ZI?

No

>> Any other suggestions to debug this issue?

Check the SPI bus with a scope to see what is happening.

 

You have an "SDCARD over SPI" example in the STM32H7 software package:

STM32H7 software package 

under:

Projects\NUCLEO-H743ZI\Applications\FatFS\FatFS_uSD_Standalone

It should be compatible with H753.

Perhhaps you'll have to change the SPI instance and the SPI pins.