Skip to main content
KTrot.1
Associate II
December 3, 2020
Solved

STPTIC tunable capacitor DC Ground

  • December 3, 2020
  • 7 replies
  • 1945 views

Hi.

I have the STPTIC-82G2 tunable capacitor, and I have noticed that there is no ground pin. What is the DC ground that the bias pin is referenced to? Should I provide DC ground through RF1/RF2 pins?

Thank you!

This topic has been closed for replies.
Best answer by JPROO.1

0693W000006EqvQQAS.jpg

7 replies

JPROO.1
ST Employee
December 3, 2020

Hello,

There is No GND pin, for Bias pin reference you should provide DC ground return through RF1 or RF2

No matter which one as they are DC connected internally in the PTIC

Best Regards

jean-pierre.proot@st.com

KTrot.1
KTrot.1Author
Associate II
December 6, 2020

Thanks for the answer!

Does that mean that RF1 and RF2 are DC shorted? What happens if they are DC biased with different voltages? Should I avoid it?

JPROO.1
ST Employee
December 7, 2020

RF1 and RF2 are not DC shorted, you have to connect RF1 or RF2 to DC ground thru a shunt inductor for instance.

If you bias RF1 or RF2 to a DC voltage (reference) then this reference will be substracted from the Vbias (Vbias - reference)

Hope it answers you question

KTrot.1
KTrot.1Author
Associate II
December 7, 2020

If, for example, RF1 is biased at 5V DC, and RF2 is biased at 3V DC, what will the be reference voltage to the "bias" pin?

JPROO.1
ST Employee
December 7, 2020

Please see internal schematic

if RFin and RFout are not using the same DC voltage there will be leakage current

JPROO.1
JPROO.1Best answer
ST Employee
December 7, 2020

0693W000006EqvQQAS.jpg

KTrot.1
KTrot.1Author
Associate II
December 7, 2020

Thanks a lot!