Skip to main content
Associate
October 16, 2023
Question

stwlc98 TX mode

  • October 16, 2023
  • 4 replies
  • 1614 views

What steps are required to set stwlc98 to TX mode?

If you set 0x0020 to 01, 0x000E becomes 03.

However, AC1 and AC2 do not cause burst oscillation.

The Optional (TX mode only) circuit is on the board, and VOUT is connected to 5V.

4 replies

Visitor II
November 14, 2023

I have the same question, I connected VOUT to 12V in my project.

The receiver was verified with other solution.

Hoping someone can answer this.

HisanoriAuthor
Associate
January 25, 2024

This issue is still unresolved.Please tell me the solution.

Associate II
April 16, 2024

Hello,

Is there alreadya solution for this problem? Is there any application note or some other more detailed description for the TX mode?

 

My problem is the following:

I want to transmit 15W, but the STWBC86 can only transmit 5W. So I have to deal with the STWBC2-HP, but this one is too big for my application and has too much functionality I do not need.

 

Thank you
Simon

Technical Moderator
April 23, 2024

STWLC98 support TX mode, please check this link at page 44 5.15 Transmitter (Tx) mode

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
April 23, 2024

Thank you, but do you have more Information how I can set up the software correctly, to get the TX mode working?