Support on SLVU2.8‑8A1
- April 24, 2026
- 1 reply
- 99 views
Hi,
We are using the ST Micro Devices SLVU2.8‑8A1 TVS array on the primary side of the Ethernet connector for ESD protection in a 1000BASE‑T Ethernet design.
It is observed that when the SLVU2.8‑8A1 is mounted, the 1G Ethernet link reports FCS errors with ~100-metre cables, whilst shorter-length cables work error-free.
When the device is removed, the Ethernet link becomes fully stable and error‑free on the same hardware with longer length cables.
Ideally the device should not interact with the Ethernet data being transmitted. Please check how the device can interact with normal datalink propagation. The problem is observed in designs with PHYs from two leading manufacturers.
Attaching the images of the device as well.
Thanks & Regards,
Rohit Dixit