Skip to main content
Associate
December 10, 2024
Solved

TDA7266D13TR Temperature specification related

  • December 10, 2024
  • 2 replies
  • 804 views

Hi ST Team
I have a question about the TDA7266D13TR product.
Checking the TDA7266D13TR datasheet gives the specifications for the TDA7266D and lists the operating temperature as 0°C to 70°C.
The temperature specification I need is -20~85°C or higher.
Please let me know if there are other options based on temperature.

Best answer by AScha.3

So for having only 10W : depends on your power supply voltage in first place.

supply is ..?

Maybe TDA7379 , AB , 4 x 11W (at 18V);

Mouser: 511-E-TDA7379

AScha3_0-1733824573343.png

https://agelectronica.lat/pdfs/textos/T/TDA7379.PDF

 

2 replies

AScha.3
Super User
December 10, 2024

Hi,

> temperature specification I need is -20~85°C or higher

So take some chip with "automotive" characteristics, maybe TDA7377 ;

-> 

AScha3_0-1733820004853.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
skybubleAuthor
Associate
December 10, 2024

Thank you for your kindness.

Since we plan to use two 10W 4ohm output speakers, it is difficult to use for products with an AMP output exceeding 10W.
Also, due to noise issues, we are only considering ABclass type.

Due to PCB area and height issues, I selected TDA7266D considering lower heat dissipation, but I am concerned about temperature issues.

AScha.3
AScha.3Best answer
Super User
December 10, 2024

So for having only 10W : depends on your power supply voltage in first place.

supply is ..?

Maybe TDA7379 , AB , 4 x 11W (at 18V);

Mouser: 511-E-TDA7379

AScha3_0-1733824573343.png

https://agelectronica.lat/pdfs/textos/T/TDA7379.PDF

 

"If you feel a post has answered your question, please click ""Accept as Solution""."