Skip to main content
ABouk.1
Associate III
January 20, 2022
Question

Teseo LIV3R connected to 3.3v but it does not send any commands, 1PPS always 0 and the module consumes 6 mA.

  • January 20, 2022
  • 1 reply
  • 1162 views

..

    This topic has been closed for replies.

    1 reply

    ABouk.1
    ABouk.1Author
    Associate III
    January 20, 2022

    Vbatt and Vcc are both connected to a power supply that provides 3.3v.

    Vcc_io is always connected to 3.3v (the same as the MCU) with a 22R resistor

    RST, wakeup, 1PPS, TX and RX are connected to the MCU, however, the module does not send 11s pulses on 1PPS and it consumes 5.6 mA all the time.

    RF_IN is connected to an active antenna and a LC circuit to provide the 3.3v.

    I am really confused, No wrong connection have been made, is it possible that the module needs to be flashed ??