Skip to main content
Associate
August 14, 2023
Solved

Testing of RF input of Teseo-VIC3DA GNSS module

  • August 14, 2023
  • 2 replies
  • 2505 views

We would like to test if the Teseo-VIC3DA module and its corresponding RF connector have been soldered correctly on the carrier board in production environment. For this it would be easiest to just apply a 1575.42 MHz continuous wave signal (un-modulated L1 carrier) to the RF connector and read out the receive signal strength from the Teseo-VIC3DA module. However, in the "Teseo-VIC3 software instructions" documentation we could not find any command for reading receive signal strength within receiver bandwidth.

Is there a method to test the module's RF input without GPS signal simulator?

This topic has been closed for replies.
Best answer by RhSilicon

Couldn't this project from the link below be used for testing?

GPS-SDR-SIM generates GPS baseband signal data streams, which can be converted to RF using software-defined radio (SDR) platforms, such as ADALM-Pluto, bladeRF, HackRF, and USRP.

https://github.com/osqzss/gps-sdr-sim

Perhaps the GPS signal needs some variation to pass through the system stages, a fixed carrier signal could be like a muted radio signal:

erEHL

https://electronics.stackexchange.com/questions/353664/gps-noise-figure-analysis

dia-gps-sig-simulator-nse-ae

How to Simulate a GPS Signal

A GPS signal simulator mimics the radio frequency (RF) operation of a GPS satellite. Digital modulation techniques are used to multiply, mix, and combine the output of a central 10.23 MHz master clock in stages to simulate a space vehicle (SV) broadcast.

A GPS satellite constellation simulator configures key variables into pre-programmed or customized test scenarios without ever leaving the test bench. This includes the quantity and position of satellites, power levels, transmission band(s), constellation health, and almanac data.

A GPS walking simulator is established by adapting signal transit times along with refection and interference settings to simulate a receiver in motion. The trajectory of incoming signals can also be adjusted to approximate SV orbits.

GPS record and replay capabilities capture output from live satellite antennas at a high rate of speed. These functions combine the authenticity of actual satellite signals with the flexibility of on-demand testing.

https://www.viavisolutions.com/en-uk/products/gps-signal-simulators

2 replies

RhSilicon
RhSiliconBest answer
Lead
August 15, 2023

Couldn't this project from the link below be used for testing?

GPS-SDR-SIM generates GPS baseband signal data streams, which can be converted to RF using software-defined radio (SDR) platforms, such as ADALM-Pluto, bladeRF, HackRF, and USRP.

https://github.com/osqzss/gps-sdr-sim

Perhaps the GPS signal needs some variation to pass through the system stages, a fixed carrier signal could be like a muted radio signal:

erEHL

https://electronics.stackexchange.com/questions/353664/gps-noise-figure-analysis

dia-gps-sig-simulator-nse-ae

How to Simulate a GPS Signal

A GPS signal simulator mimics the radio frequency (RF) operation of a GPS satellite. Digital modulation techniques are used to multiply, mix, and combine the output of a central 10.23 MHz master clock in stages to simulate a space vehicle (SV) broadcast.

A GPS satellite constellation simulator configures key variables into pre-programmed or customized test scenarios without ever leaving the test bench. This includes the quantity and position of satellites, power levels, transmission band(s), constellation health, and almanac data.

A GPS walking simulator is established by adapting signal transit times along with refection and interference settings to simulate a receiver in motion. The trajectory of incoming signals can also be adjusted to approximate SV orbits.

GPS record and replay capabilities capture output from live satellite antennas at a high rate of speed. These functions combine the authenticity of actual satellite signals with the flexibility of on-demand testing.

https://www.viavisolutions.com/en-uk/products/gps-signal-simulators

eDesignerAuthor
Associate
September 5, 2023

Hello RhSilicon. We now used your proposed approach with ADALM-Pluto SDR, together with the gpr-sdr-sim and plutoplayer_win software. This worked fine, but only after providing a frequency-accurate external reference clock to the Pluto using a signal generator from R&S.

We want to replace the internal crystal oscillator of the Pluto with one that is frequency-accurate enough for GPS signal simulation. What is the required frequency accuracy in ppm for the simulated GPS signal for the Teseo-VIC3DA modules?