Solved
USB issue with STM32F411
- August 6, 2023
- 2 replies
- 1847 views
This has nothing to do with EEPROM devices, but that was the only "labeI" that would work. I built a custom board using an STM32F411RET6. It has a 12MHz external clock. I'm trying to use a VCP USB interface. The USB code enumerates fine on a 'F407 DISCO board (STM3240G-EVAL), of course with the 25MHz crystal instead of my 12MHz oscillator. But I get the attached USB connection error with my custom board. This interface won't allow me to attach a .zip of my code, and only 3 attachments are allowed, but I can send the CubeMX file I am using, and the actual code.