Skip to main content
CCenc.1
Visitor II
March 10, 2022
Question

VL53L1x communication with STM8S105 MCU

  • March 10, 2022
  • 3 replies
  • 2639 views

Dear all,

I have just put the X-NUCLEO-53L1A1 kit into operation together with Arduino UNO and everything works perfectly, using the "X_NUCLEO_53L1A1_HelloWorld" application package.

Then I mounted one of the same two VL53L1X-SATEL sensors by interfacing it with the STM8S MCU, using the "VL53L1X ULD API" application package, but here I still have a basic problem that I can't explain.

Before sending the FW used, based on the following flow:

0693W00000Kc552QAB.jpgI would like to briefly describe the defect found in the "VL53L1X_GetInterruptPolarity" function, called within "VL53L1X_CheckForDataReady", in turn called within "VL53L1X_SensorInit".

The problem is that in the following function:

VL53L1X_ERROR VL53L1X_CheckForDataReady (uint16_t dev, uint8_t * isDataReady)

{

uint8_t Temp;

uint8_t IntPol;

VL53L1X_ERROR status = 0;

status | = VL53L1X_GetInterruptPolarity (dev, & IntPol);

status | = VL53L1_RdByte (dev, GPIO__TIO_HV_STATUS, & Temp);

/ * Read in the register to check if a new value is available * /

if (status == 0) {

if ((Temp & 1) == IntPol)

* isDataReady = 1;

else

* isDataReady = 0;

}

return status;

}

equality (Temp & 1) == IntPol IS NEVER VERIFIED !!!

Just to remember:

L53L1X_ERROR VL53L1X_GetInterruptPolarity(uint16_t dev, uint8_t *pInterruptPolarity)

{

uint8_t Temp;

VL53L1X_ERROR status = 0;

status |= VL53L1_RdByte(dev, GPIO_HV_MUX__CTRL, &Temp);

Temp = Temp & 0x10;

*pInterruptPolarity = !(Temp>>4);

return status;

}

Comparing with the oscilloscope the I2C bytes exchanged in the working case of Arduino UNO and in the non-working case STM8S105, we have the following:

  • Arduino UNO "VL53L1X_GetInterruptPolarity":

0693W00000Kc5OiQAJ.bmp 

  • STM8S105 "VL53L1X_GetInterruptPolarity":

0693W00000Kc5P7QAJ.bmp 

Comparing to Arduino UNO we expect to read the byte 0x01 from the register GPIO_HV_MUX__CTRL, but on STM8S105 we always read 0x11!!!

Due to this problem we have always been stuck inside the function without being able to receive any distance measurement data since dataReady == 0 ALWAYS TRUE !!! (data NEVER READY)

Please, anyone have experience with VL53L1X ULD implemented on STM8S MCU?

I can provide other details if necessary.

I would be very grateful.

Thanks.

CCenci

PS. Just to remember from ULD on STM8S105:

VL53L1X_ERROR VL53L1X_SensorInit(uint16_t dev)

{

VL53L1X_ERROR status = 0;

uint8_t Addr = 0x00, tmp;

for (Addr = 0x2D; Addr <= 0x87; Addr++)

status |= VL53L1_WrByte(dev, Addr, VL51L1X_DEFAULT_CONFIGURATION[Addr - 0x2D]);

status |= VL53L1X_StartRanging(dev);

tmp = 0;

while(tmp==0)

status |= VL53L1X_CheckForDataReady(dev, &tmp);

status |= VL53L1X_ClearInterrupt(dev);

status |= VL53L1X_StopRanging(dev);

status |= VL53L1_WrByte(dev, (uint16_t)VL53L1_VHV_CONFIG__TIMEOUT_MACROP_LOOP_BOUND, 0x09); /* two bounds VHV */

status |= VL53L1_WrByte(dev, (uint16_t)0x0B, 0); /* start VHV from the previous temperature */

return status;

}

This topic has been closed for replies.

3 replies

AVarg.7
Visitor II
April 13, 2022

Same issue on atmel SAML based board!

ESmel.1
Visitor II
June 8, 2022

Same issue

you found a solution?

i use TOF400F

AVarg.7
Visitor II
June 8, 2022

Not entirely sure, but the following worked for us.

The issue was probably with the power drawn by the module. Had to ensure that the VDD was connected to 3.3V supply with enough capacity for 20mA+ current draw.

We had earlier tried to power it off a GPIO pin of the microcontroller and every-time we did that, it did not work and gave dataReady ==0 all the time.