Skip to main content
AFidi.1
Associate II
January 28, 2023
Solved

X-CUBE-GNSS1 only shows minute part of coordinates

  • January 28, 2023
  • 1 reply
  • 1184 views

I'm using ST's X-CUBE-GNSS1 software pack but it only prints the minute part of my location coordinate

0693W00000Y9O1WQAV.pngCompared with the actual coordinate that shows the degree and seconds part

0693W00000Y9O1gQAF.pngHere's the software pack code that correspond with the above output

void GNSS_DATA_GetGPRMCInfo(GNSSParser_Data_t *pGNSSParser_Data)
{
 PRINT_INFO("\r\n");
 
 (void)snprintf((char *)msg, MSG_SZ, "UTC:\t\t\t\t[ %02d:%02d:%02d ]\n\r",
 pGNSSParser_Data->gprmc_data.utc.hh,
 pGNSSParser_Data->gprmc_data.utc.mm,
 pGNSSParser_Data->gprmc_data.utc.ss);
 PRINT_INFO((char *)msg);
 
 (void)snprintf((char *)msg, MSG_SZ, "Status:\t\t\t\t[ %c ]\t\t",
 pGNSSParser_Data->gprmc_data.status);
 PRINT_INFO((char *)msg);
 if (pGNSSParser_Data->gprmc_data.status == (uint8_t)'A')
 {
 PRINT_INFO("-- Valid (reported in 2D and 3D fix conditions)\n\r");
 }
 else if (pGNSSParser_Data->gprmc_data.status == (uint8_t)'V')
 {
 PRINT_INFO("-- Warning (reported in NO FIX conditions)\n\r");
 }
 else
 {
 PRINT_INFO("-- Unknown status\n\r");
 }
 
 float64_t lat_mod = fmod(pGNSSParser_Data->gprmc_data.xyz.lat, 100.0);
 float64_t lon_mod = fmod(pGNSSParser_Data->gprmc_data.xyz.lon, 100.0);
 
 (void)snprintf((char *)msg, MSG_SZ, "Latitude:\t\t\t[ %f' %02d'' %c ]\n\r",
 (pGNSSParser_Data->gprmc_data.xyz.lat - lat_mod) / 100.0,
 (int16_t)lat_mod,
 pGNSSParser_Data->gprmc_data.xyz.ns);
 PRINT_INFO((char *)msg);
 
 (void)snprintf((char *)msg, MSG_SZ, "Longitude:\t\t\t[ %f' %02d'' %c ]\n\r",
 (pGNSSParser_Data->gprmc_data.xyz.lon - lon_mod) / 100.0,
 (int16_t)lon_mod,
 pGNSSParser_Data->gprmc_data.xyz.ew);
 PRINT_INFO((char *)msg);
 
 (void)snprintf((char *)msg, MSG_SZ, "Speed over ground (knots):\t[ %.01f ]\n\r",
 pGNSSParser_Data->gprmc_data.speed);
 PRINT_INFO((char *)msg);
 
 (void)snprintf((char *)msg, MSG_SZ, "Trackgood:\t\t\t[ %.01f ]\n\r",
 pGNSSParser_Data->gprmc_data.trackgood);
 PRINT_INFO((char *)msg);
 
/*
 (void)snprintf((char *)msg, MSG_SZ, "Date (ddmmyy):\t\t\t[ %ld ]\n\r",
 pGNSSParser_Data->gprmc_data.date);
*/ /* Replaced by the following implementation for compatibility with AC6 and gcc compilers */
 (void)snprintf((char *)msg, MSG_SZ, "Date (ddmmyy):\t\t\t[ %02d%02d%02d ]\n\r",
 (int16_t)((pGNSSParser_Data->gprmc_data.date/10000)),
 (int16_t)((pGNSSParser_Data->gprmc_data.date/100) - (100*(pGNSSParser_Data->gprmc_data.date/10000))),
 (int16_t)(pGNSSParser_Data->gprmc_data.date - (100*(pGNSSParser_Data->gprmc_data.date/100))));
 PRINT_INFO((char *)msg);
 
 (void)snprintf((char *)msg, MSG_SZ, "Magnetic Variation:\t\t[ %.01f ]\n\r",
 pGNSSParser_Data->gprmc_data.mag_var);
 PRINT_INFO((char *)msg);
 
 if ((pGNSSParser_Data->gprmc_data.mag_var_dir != (uint8_t)'E') &&
 (pGNSSParser_Data->gprmc_data.mag_var_dir != (uint8_t)'W')) {
 (void)snprintf((char *)msg, MSG_SZ, "Magnetic Var. Direction:\t[ - ]\n\r");
 }
 else {
 (void)snprintf((char *)msg, MSG_SZ, "Magnetic Var. Direction:\t[ %c ]\n\r",
 pGNSSParser_Data->gprmc_data.mag_var_dir);
 }
 PRINT_INFO((char *)msg);
 
 PRINT_INFO("\n\n\r>");
 
 return;
}

How do I print the other two components of the coordinate?

    This topic has been closed for replies.
    Best answer by waclawek.jan

    You probably don't have enabled printing of float. Search this forum or internet (-u _printf_float).

    JW

    1 reply

    waclawek.jan
    waclawek.janBest answer
    Super User
    January 28, 2023

    You probably don't have enabled printing of float. Search this forum or internet (-u _printf_float).

    JW

    AFidi.1
    AFidi.1Author
    Associate II
    January 28, 2023

    Woops! totally forgot about that. Thanks!