Skip to main content
Visitor II
November 8, 2025
Question

Are the TLV2372's surroundings and pin connections correct ?

  • November 8, 2025
  • 1 reply
  • 174 views

STM32F030F4P6TR'nin PA5 pininde PWM araştırmaları. TLV2372ID ile 0-10V analog çıkış elde etmeyi planlıyorum. Devre şemasının doğru olması gerekiyor. TLV2372'nin sınırları ve pin bağlantıları doğru mu?

1 reply

Peter BENSCH
Technical Moderator
November 9, 2025

English is not my native language either, but it is the language of communication defined by the community, which is why I am responding in English here.

For 0...10V, an opamp with approximately three times the gain is required (3.03, to be precise) if you have a VCC of 3.3V. According to the connection diagram, you have wired it correctly, although a drawing of opamps with a classic triangle would be clearer and better readable for the supporters here.

Please note: even though the TLV2372 is an RRIO opamp, it will output a significant output voltage of approx. 200mV at a VDD of 12V and very low input voltages close to 0.

Good luck!

Regards
/Peter