Beginner; make STM32F407 DevEBox available in Arduino IDE
Hi, I bought an DevEBox STM32F407 board to experiment with, using it as an Arduino on steroids. I installed al the required stuff in the Arduino IDE and I now have this board available there. But Windows 11 does not know what to do with the board when hooked up via USB. There is no COM port available in Arduino and the devide manager sees something, but has no drivers for it. I installed some drivers I found googling, but to no avail. I have the BT0 and 3V3 pins connected when I connect the board, if I don't Windows thinks of the board is a USB drive. With the jumper in place, device manager calls it STM32 BOOTLOADER, but as said it doesn't know what to do with it. Please advise.
Cheers,
Hugo