Bug found while using the REG_Access block from the MAT/TARGET Library
Hi,
I use the REG_Access block to read the value stored in the data register of the SPI1. So I change the 'Peripheral' option from NVIC to SPI1.
But it always goes back to NVIC, once the the simulink model is closed and reopened again. If I don't notice this change and don't manually set it again, it will lead to errors while compiling the code in the IDE.
My software versions are as below:
MATLAB: R2017a
STM32 MAT/TARGET Library: 4.4.2
Best Regard,
qxj
#stm32-mat/target-matlab #simulink