Skip to main content
RZhu
Visitor II
September 12, 2019
Question

Can the EEPROM Emulation be used on STM32F446?

  • September 12, 2019
  • 2 replies
  • 1284 views

The Application note AN3969 describes a software solution for EEPROM Emulation on STM32F40x/STM32F41x devices.But it haven't mentioned that it can worked on other STM32F4 devices or not.

So,can the EEPROM Emulation be used on STM32F446 or other STM32F4 devices?

https://www.st.com/content/ccc/resource/technical/document/application_note/ec/dd/8e/a8/39/49/4f/e5/DM00036065.pdf/files/DM00036065.pdf/jcr:content/translations/en.DM00036065.pdf

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
September 12, 2019

The flash sectors on the F446 should be organized in the same way as those on the F40x devices.

If you can avoid the emulation, and use flash directly, that would be advisable.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Dejan Nedeljkovic
Associate III
September 24, 2019

Hi @Community member​ 

Why is it better to use the flash directly instead of eeprom emulation?

I'm getting some hardfualts with the emulation when calling FLASH_Erase_Sector() on STM32F767II.

This is why I also thought of using directly the flash without the eeprom emulation.

Regards

Dejan