code crashes and lead to Hardfault when I include I2C1_IRQ_handler.
Hi guys,
I using
keil uvisionV5.35.0.0
arm_compiler : V6.16
We are developing a project on STM32L071CZYx MCU. which has
flash memory: 192kB
RAM: 20KB
I have attached a I2C1_IRQhandler function for your reference.
void I2C1_IRQHandler(void)
{
I2C1->CR1 &= ~(I2C_CR1_RXIE |I2C_CR1_ADDRIE | I2C_CR1_STOPIE | I2C_CR1_TXIE);
switch((I2C1->ISR &(I2C_ISR_STOPF | I2C_ISR_ADDR |I2C_ISR_RXNE | I2C_ISR_TXIS)))
{
case 0x08: //address match
dev_addr = ((I2C1->ISR >> 16 ) & 0xFE); // assigning Recieved slave address
if(I2C1->ISR & I2C_ISR_DIR)
{
// Slave address with Read bit
if(i2c_state == I2C_GOT_CONTROL_WORD_ADDR)
{
i2c_state = I2C_REPEATED_START;
}
else
{
i2c_state = I2C_RD_STARTED;
}
__HAL_I2C_CLEAR_FLAG(&hi2c1,(I2C_FLAG_ADDR ));
I2C1->CR1 |= (I2C_CR1_TXIE); // enabling Transmitter Interrupt
//slave Tx
}
else
{
// Slave address with write bit
i2c_pkt_length = 0;
i2c_state = I2C_WR_STARTED;
__HAL_I2C_CLEAR_FLAG(&hi2c1,I2C_FLAG_ADDR);
I2C1->CR1 |= (I2C_CR1_RXIE); // stopIE is not required
//slave Rx
}
break;
case 0x04: //rx data for master
if(i2c_state == I2C_WR_STARTED)
{
CW =I2C1->RXDR;
word_addr = CW;
i2c_state = I2C_GOT_CONTROL_WORD_ADDR;
}
else
{
i2cdatarx[i2c_pkt_length++] = I2C1->RXDR;
i2c_state = I2C_DATA_STARTED;
}
__HAL_I2C_CLEAR_FLAG(&hi2c1,I2C_FLAG_RXNE);
I2C1->CR1 |= (I2C_CR1_RXIE | I2C_CR1_ADDRIE | I2C_CR1_STOPIE); // enabling Rx address match and Stop interrupt
break;
case 0x20: // detected a stop
if (dev_addr == 0xB0 )
{
if (i2c_state == I2C_DATA_STARTED || i2c_state == I2C_GOT_CONTROL_WORD_ADDR)
{
F0_write(word_addr);
}
else
{
I2C1->ISR |= I2C_ISR_TXE;//Setting flushing the TX buffer for new data transfer
}
}
else
{
if (i2c_state == I2C_DATA_STARTED || i2c_state == I2C_WR_STARTED)
{
if (mode == mFACTORY)
{
A0_write_FM(word_addr); // writting to sram and Eeprom
}
else
{
A0_write(word_addr);
}
}
else
{
I2C1->ISR |= I2C_ISR_TXE;//Setting flushing the TX buffer for new data transfer
}
}
i2c_state = I2C_IDLE;
__HAL_I2C_CLEAR_FLAG(&hi2c1,I2C_FLAG_STOPF);
I2C1->CR1 |= (I2C_CR1_ADDRIE); // enabling address match
break;
case 0x02: // Transmit has detected
//i2cdatarx = I2C_read_F0(CW);
if (dev_addr == 0xB0)
{
I2C1->TXDR = F0_Read(CW);
}
else
{
if (mode == 1)
{
I2C1->TXDR = A0_read_FM(CW);
}
else
{
I2C1->TXDR = A0_read(CW);
}
}
__HAL_I2C_CLEAR_FLAG(&hi2c1,(I2C_FLAG_ADDR));
I2C1->CR1 |= (I2C_CR1_STOPIE | I2C_CR1_TXIE);
break;
}
}here I2C1 is configured has a slave.
without I2C_IRQ_handler function I2C1 will work well in polling mode.
Code crashes and lead to hardfault at hsc_dev_obj_init when I include I2C1_IRQ_handler function.
I have tried all the ways like increasing stack memory and reducing global variables but nothing works. please help me to resolve this error.
Regards,
Gopal Gowda