Question
Configure LoRa E22-900M22s module and MAX3485 (for Rs485) into STM32H753ZIT6
Hi, I am working on configuring LoRa (E22-900M22S) and the MAX3485 transceiver to establish RS-485 communication using the STM32H753ZI. I have connected the LoRa and MAX3485 modules as per the following reference:
| LoRa(E22-900M22S) | |
| LoRa Pin | STM32H753ZI Pin (example) |
| MOSI | PA7 (SPI1_MOSI) |
| MISO | PA6 (SPI1_MISO) |
| SCK | PA5 (SPI1_SCK) |
| NSS | PA4 (GPIO) |
| RESET | PB0 (GPIO) |
| DIO1 | PB1 (EXTI-capable GPIO) |
| DIO2 | PB2 (EXTI-capable GPIO) |
| BUSY | PB10 (GPIO input) |
| GND | GND |
| VCC | 3.3V |
| RS-485(MAX3485) | |
| STM32H753ZI Pin | MAX3485 Pin |
| PD8 | DI |
| PD9 | RO |
| PD12 (or any GPIO with DE support) | DE + RE (tied together) |
| 3.3V | VCC |
| GND | GND |
Could you please guide me on how to configure both LoRa and RS-485 communication using STM32CubeIDE?