Dallas iButton and UART
Hi there!
i start to work with Dallas Ibutton and for my project i use STM32G031K8 nucleo. Because i need to read only one ibutton i use the UART peripheral and no ic dedicate for 1Wire. My problem is when i try to use the rx callback function for know when i receive all data (and i start wit receive one bit at the time) never shoot, If i put a simple delay of 1ms everythingh wor very well i can see all my data on my logic analyzer .Question because the nucleo use the second uart2 for debug is possible that give me the problem ? and if yes how can i resolve ?
Thank you soo much
Sergio