Though I made sure that the STM32 NUCLEO-U545RE-Q device was connected to CubeProgrammer, MATLAB Simulink is unable to read it. Any help that can be provided will be appreciated! I appreciate any help you can provide.
Though I made sure that the STM32 NUCLEO-U545RE-Q device was connected to CubeProgrammer...
So STM32CubeProgrammer can connect & works OK ?
Does MATLAB require that you disconnect the CubeProgrammer first ?
If CubeProgrammer connects OK, but MATLAB can't, then it's a MATLAB issue - as @STTwo-32 said, you need to contact MATLAB in that case.
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.