External Flash for STM32F439Zi
Dear Sir/Madam,
Good day~
I am currently using STM32F439ZI for the purpose of developing BMS.
However, the code size exceed the internal Flash capacity, which is 2MB.
To address this, I intend to add an external Flash (MXIC:MX25L25645G).
May I know whether the external Flash can connect to any of the six SPIs available on the STM32F439ZI?
or there are specific SPIs for interfacing with external Flash?
Any guidance would be appreciated.
Vince