FLASH SR error set after clearing TIM interrupts before timer initialization
When using a TIM timebase (rather than systick), the PGSERR bit in the FLASH.SR register gets set after calling HAL_InitTick. Using the debugger, I found that the specific line that causes the flash error is "__HAL_TIM_CLEAR_IT(htim, TIM_IT_CC2)". This appears to be the case when using different timers as the timebase as well.
I am using STM32CubeIDE 1.7.0, STM32Cube FW_G4 V1.4.0, and GNU Tools for STM32 (9-2020-q2-update). My target is the Nucelo G431RB.