Skip to main content
Visitor II
November 3, 2025
Question

getting started with the Morse Micro MM8108-EKH and STM32CubeIDE

  • November 3, 2025
  • 1 reply
  • 207 views
I'm attempting to get started with the Morse Micro MM8018-EKH05 (STM32U585VIT6 controlled) and pair it with their HaloLink1 router.  I am following their MM8108-EKH05 used guide user guide section "5.2 Build and Run Example Applications." I have loaded the downloaded CMSIS package with STMCubeIDE,  imported the project, loaded the MM8108 software packs, generated code in STMCubeIDE, and built but when I get to the green "Run" phase on pg. 29, I get the following error (see attached screenshots):   
 
Cannot run program "C:\Users\dmitryp\STM32Cube\Repository\Packs\MorseMicro\MM_IoT\1.7.4\HaLow_example_spi\Debug\HaLow_example_spi.elf": Launching failed
Cannot run program "C:\Users\dmitryp\STM32Cube\Repository\Packs\MorseMicro\MM_IoT\1.7.4\HaLow_example_spi\Debug\HaLow_example_spi.elf": Launching failed
Cannot run program "C:\Users\dmitryp\STM32Cube\Repository\Packs\MorseMicro\MM_IoT\1.7.4\HaLow_example_spi\Debug\HaLow_example_spi.elf": Launching failed
 
What should I change in order to clear the errors so I can flash the board?  Is there a directory change somewhere or maybe the STM32Cube folder needs to be changed to STMCube32IDE or combine the folders into one?  I just want the EKH05 board to communicate with the HaloLink 1 router somehow (preferably wirelessly) so I can have a starting point of what to do next.  Thanks.

1 reply

Andrew Neil
Super User
November 3, 2025

Welcome to the forum.

Please see  How to write your question to maximize your chances to find a solution for best results.

 


@Dima587 wrote:
I'm attempting to get started with the Morse Micro MM8018-EKH05

Did you mean MM8108-EKH05-01 ?

It's not an ST board, so Morse Micro should be your first point of call for support with their product:

https://www.morsemicro.com/dashboard/

https://community.morsemicro.com/

 

Your screenshots are a bit small to read!

If you just want to program the board and let it run - not debug - try STM32CubeProgrammer.

To debug, use a Debug configuration rather than 'Run'.

Are you sure that the ST-Link is properly seen by your PC?

Here are ST's tips for debugger problems:

How to solve connection errors when connecting and programming the STM32 target board.

How to solve debugger connection issues;

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.