Hi, I am trying to program a Nucleo64 (STM32L476) with Arduino IDE.
In my code for Arduino101, I use the following:
#include "CurieTimerOne.h"
This is the point where I get an error when I use Nucleo64 STM32L476. I have no problem when I use Arduino101. However, a problem arises with Nucleo where it cannot find this library.
The error message while using Nucleo is:
MyFileName:50:10: fatal error: CurieTimerOne.h: No such file or directory
50 | #include "CurieTimerOne.h"
| ^~~~~~~~~~~~~~~~~
compilation terminated.
I downloaded this library from Github and added it to the existing libraries' folder but no success!
Whatever I do with the sub folders included in this library and other dependencies, I cannot fix this problem.
Any help is appreciated.