How to connect STM32 Virtual COM Port (USB CDC) to RS485 bus using external converter
Hi,
I’m using an STM32L412RB where the USB DM/DP lines are already configured as a Virtual COM Port (USB CDC device).
Now I want to communicate with an RS485 bus without changing the existing board hardware.
My idea is to build a small adapter board that connects the STM32 USB DM/DP pins to an external USB-to-RS485 converter (which has DM and DP lines).
Is it possible to design such an adapter to convert the STM32’s USB VCP interface to RS485?
Can the STM32 (configured as a USB device) send and receive RS485 data through this path:
STM32 (USB CDC Device) → USB DM/DP → USB-to-RS485 Converter → RS485 Bus
Any guidance or reference designs would be helpful.
Thanks,
Sujith