Skip to main content
Associate
November 15, 2024
Question

Issue with DNS resolution on STM32F407G and SIM7600 GSM module (using PPPOS)

  • November 15, 2024
  • 0 replies
  • 1009 views

I’m working on a project using an STM32F407G and a SIM7600 GSM module. After successfully sending AT commands via UART to configure the GSM module, I switched to PPPOS. I’m able to get a valid IP address, gateway, and netmask from the modem:

 

GSM: LTE_ppposInit
GSM: status_cb: Connected
GSM: ipaddr = 100.73.194.248
GSM: gateway = 10.64.64.64
GSM: netmask = 255.255.255.255

However, I’m encountering an issue with DNS resolution. Using netconn_gethostbyname, I can successfully resolve the IP for a hostname. But when I try using dns_gethostbyname, it fails with a DNS resolution error. The DNS server is correctly set (e.g., 1.1.1.1), but for some reason, dns_gethostbyname doesn’t work as expected. Here’s part of my code:

 

void dns_callback(const char *name, const ip_addr_t *ipaddr, void *arg) {
 if (ipaddr != NULL) {
 printf("Resolved IP: %s\n", ipaddr_ntoa(ipaddr)); 
} else {
 printf("DNS resolution failed\n"); 
}
 }


void resolve_hostname() {
ip_addr_t resolved_ip;
dns_init();
err_t err = dns_gethostbyname("test.mosquitto.org", &resolved_ip, dns_callback, NULL);
if (err == ERR_OK) {
printf("Resolved IP immediately: %s\n", ipaddr_ntoa(&resolved_ip));
} else if (err == ERR_INPROGRESS) {
printf("DNS resolution in progress\n");
} else {
printf("DNS resolution error: %d\n", err);
}
}

 


Any advice on why dns_gethostbyname might be failing even though netconn_gethostbyname works fine?