Associate II
September 16, 2019
Solved
LED blinking using Simulink and STM32-MAT/TARGET not working
- September 16, 2019
- 13 replies
- 3156 views
I have installed STM32-MAT/TARGET , generated configuration with CubeMx, made simulink model, generated c code for keil, and compiled with out errors but the port is not toggling. I have been trying for last two weeks to get it work. I have attached cubemx file and simulink model with this message, kindly someone help me
Matlab2019a
STMcubeMx 5.3
I have tried with the simpleGPIO example supplied also, but that too didn't worked, is there any compatibility issue between the cubeMX and Matlab2019 version?
The examples supplied are made with earlier version of cubeMX and Matlab