Associate
June 2, 2025
Question
Low power small display to use with STM32L0
- June 2, 2025
- 2 replies
- 333 views
Hi All,
I am looking for a small 4-5 digit monochrome display to use with STM32L0 series in a coin cell powered application. Actually the display I am searching is similar to the ones used in kids watch or small temperature or humidity meters. I only need to display time or a 3 digit counter. I prefer to have wires or pins instead of the glass display with conducting rubber alignment and the length of the display should be less than 3cm. It is really hard to find even how to search for this display. It would be really great if someone can help with this.
Attaching an image as an example.
Thanks in advance,
Best regards