Nucleo-H753ZI board Connect ADC inputs to GND, the readings are varied between -15 - +15
Nucleo-H753ZI board. ADC1 configurations: INPUT: SINGLE-END
Sample clock rate = 5Mhz
Sample rate = 10Khz,
Sample Time = 16.5 cycles,
Resolution = 12-bit
Scan 256 times
Connect the defined two ADC input channels to GND.
The 256 readings FOR EACH INPUT are varied between (-15 - +15), more or less, while they should be read as zeros.
Question: Can it be fixed How to fix it?
Could you do the same test to confirm it?
Thanks,
Rong