Problem with trueSTUDIO v9.3.0 not with trueSTUDIO v7.1.0
I have created a project in trueSTUDIO v7.1.0 on computer 1 and compiled it well without any errors. But when I imported the same project to trueSTUDIO v9.3.0 on computer 2 it is giving me an error.(ERROR: Program "GCC" not found in PATH ).
When I checked the PATH variable in (Properties-> C/C++ Build->Environment(PATH: C:\Program Files (x86)\Atollic\TrueSTUDIO for STM32 9.3.0\ARMTools\bin; )) .Its was fine as bin contains the arm-atollic-eabi-gcc compiler. What might be the problem? Did anyone faced the same issue? Any help will be appreciated. Thank you.:beaming_face_with_smiling_eyes: