Skip to main content
Visitor II
April 4, 2025
Question

RAK3172 Module boot mode issues

  • April 4, 2025
  • 1 reply
  • 604 views

Hello,

I hope you are doing well.

I am currently facing critical issues with my RAK3172 module and STM32Cube Programmer setup and urgently need your technical support. Here are the details:

1. RAK3172 Module Issue (LoRa P2P Communication)

  • Initially, the module booted up correctly, but now it does not enter boot mode.

  • I receive a "baud rate not detected" error when attempting to communicate.

  • The RAK Firmware Upgrade Tool fails with a device timeout error, and STM32CubeProgrammer does not work either.

  • Despite this, I can still read the firmware version from the port, so I’m unsure if the IC is damaged.

2. ST-Link & STM32Cube Programmer Issue

  • The device only connects in Hot Plug mode when I press the reset button.

  • In normal mode, it fails to connect and shows RDP Level 0.

  • Releasing the reset button causes an immediate disconnection.

  • I am unable to erase the chip, even in Hot Plug mode or while holding the reset button.

Request for Support

Could you please help me resolve these issues? Specifically:

  1. Are there any hardware requirements (e.g., resistors, connections) I might be missing?

  2. Is there a way to recover the IC or troubleshoot further?

  3. Could this indicate a hardware fault, or is it a firmware/configuration issue?

I urgently need to get this working and would greatly appreciate your prompt assistance. Please let me know the next steps or any debugging methods I should try.

Thank you in advance for your support.

Best regards,
Hetal

1 reply

Andrew Neil
Super User
April 5, 2025

@hetal wrote:

urgently need your technical support


This is primarily a user-to-user forum.

If you want direct support from ST, raise a ticket here: https://ols.st.com/s/ 

 

It's a 3rd-party module by RAKWireless - have you tried contacting them for support?

https://www.rakwireless.com/en-us/contact-us 

https://forum.rakwireless.com/

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.