Skip to main content
Visitor II
May 18, 2025
Question

Register Level Communication With EMW3080 On The B-U585I-IOT02A

  • May 18, 2025
  • 1 reply
  • 585 views

Hello,

I am currently trying to use the EMW3080 Wi-Fi chip on the B-U585I-IOT02A over SPI. I am using the Keil µVision IDE and I am trying to use a bare-metal approach without a HAL. I am trying to send data over to ThingSpeak from the temperature and humidity sensor that is built on the board. I have been having significant issues communicating with the EMW3080 over SPI. If anyone is able to provide some guidance, that would be very helpful. I am not able to get the SPI clock to generate. I do not know what SPI mode the Wi-Fi chip is, and I do not know what protocol I need to use to communicate with the chip. I have attached my main.c file.

Thanks for any help.

1 reply

mƎALLEm
Technical Moderator
October 15, 2025

Hello,

The recommendation is to use HAL and validate your hardware before moving to the bare metal programming.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."