STM32 blue pill not connecting to Arduino IDE.
Hi guys, I have a STM32 blue pill and followed instructions from a youtube video which showed me how to program the Blue pill with the Arduino IDE. After doing something I was able to load code on to it but later I wasn't able to. I am using a MacBook Pro and the Arduino is giving me an error message of this-
Arduino: 1.8.9 (Mac OS X), Board: "Generic STM32F103C series, STM32F103C8 (20k RAM. 64k Flash), Serial, 72Mhz (Normal), Smallest (default)"
Sketch uses 12648 bytes (19%) of program storage space. Maximum is 65536 bytes. Global variables use 2456 bytes (11%) of dynamic memory, leaving 18024 bytes for local variables. Maximum is 20480 bytes. Error probing interface "serial_posix" stm32flash Arduino_STM32_0.9 Cannot handle device "/dev/cu.usbserial-A800GAP3"
Failed to open port: /dev/cu.usbserial-A800GAP3http://github.com/rogerclarkmelbourne/arduino_stm32
Using Parser : Raw BINARY
the selected serial port does not exist or your board is not connected
This report would have more information with "Show verbose output during compilation" option enabled in File -> Preferences
This is the error message I get every time I hook up my Blue pill to an FTDI tool. What should I do?