STM32 OCR Project - Help choosing CAM
- April 16, 2025
- 1 reply
- 851 views
Hello,
I'm learning embedded development (junior level) and picked up a free STM32u575zit6q Nucleo Dev Board.
My goal is to build an embedded system that captures a VIN string and saves it to a .csv file. Ideally done through embedded and low level. Later I'd like to incorporate cloud systems to easily see the csv as a spreadsheet on an app or webpage and phase out the LCD/IPS display.
My main question is, how important is an FIFO for this board and would it hurt if I don't buy a camera that has one installed? What cams would be ideal for this project?
Is there a system for scanning VINs and converting them to strings easily? I was thinking of incorporating Yolo/OpenCV but not sure if this microprocessor would be powerful enough.
Any advice on my design choices?
Display:
2.4 inch SPI onilne shop factory ESP32 LCD TFT Electronic Module colorful RGB 65k ILI9341 Display 320*240
Camera Module:
b_u585i_iot02_: when looking through the projects, I noticed the STMU5 already had some camera driver support
B-CAMS-OMV Camera Module STMicroelectronics camera module (MB1379)
– Based on the OV5640 image sensor offering a 5-Mpixel resolution with 8-bit color
This however was my first choice until I noticed the importance of an FIFO for an STM32
OV7670 300KP camera module module Supports VGA CIF auto exposure control display active size 640X480 For Arduino
or the Rasp Pi/Adrucam 12 MP IMX477*
When choosing a camera module, what am I looking for? If it's DCIM or STM32 compatible or just forums and documentation?
If you could explain why both the ST cameras are HQ 5 MP but look extremely different that'd be helpful.
Thank you,
Dan (blurry)