Skip to main content
FShah.1
Associate III
June 19, 2025
Question

STM32F446 using UART4 to interface NEO M9N GPS not working

  • June 19, 2025
  • 2 replies
  • 451 views

Hi,

I am trying to interface the SparkFun Neo M9N GPS module with an STM32F446 MCU using UART4, but I am unable to receive any GPS data. Interestingly, when I switch to USART1, the module works perfectly.

Could you please help me understand why UART4 is not functioning while USART1 works fine? Additionally, I could not find any reference code for interfacing the module using I2C. If any source or example is available, it would be greatly appreciated.

Thank you!

2 replies

mƎALLEm
Technical Moderator
June 25, 2025

Hello,

Hard to tell what the problem is based on the information you provided.

What board are you using? may be also you need to share your code/project.

Make sure you set the same configuration for UART4 as for USART1. Make sure you have used the correct Tx/Rx pins for UART4.

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."
Andrew Neil
Super User
June 25, 2025

As @mƎALLEm said, you need to provide more detail - see: How to write your question to maximize your chances to find a solution.

 

Have you tested with a terminal that you can receive anything on UART4?

Have you confirmed that GPS data is actually reaching the UART4 Rx pin?

 

Some tips on debugging serial comms:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228#:~:text=tips%20specifically%20on%20Debugging%20Serial%20Comms%3A

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.