TSDHD STM32H7S7I8T6
Hello ST Community,
I am using TSD HD Gen4-STM32-43CT-01 display module which has STM32H7S7I8T6 MCU.
I am facing an issue where I am unable to connect or disconnect the debugger using MB1440C, while the same debugger works perfectly with other TSD HD Gen4 displays.
Debugger setup
Debugger: MB1440C
Interface: SWD
Connections:
SWDIO → JTMS
SWCLK → JCLK
GND → GND
This setup was working earlier on the same board.
What changed
The last firmware flashed was a boot-level application intended to write custom data into external QSPI flash:
External Flash: GD25Q127CS (128 Mbit)
After flashing this boot code:
The MCU is no longer connectable via SWD
ST-LINK / MB1440C cannot attach
Power cycling does not help
Observations
Same MB1440C debugger + same CubeIDE works fine with other TSD HD displays
Issue is specific to this board after boot code flashing
I suspect:
SWD pins may be reconfigured as GPIO
Option Bytes may have been modified
Boot code may be disabling debug or putting MCU in low-power/reset loop
External QSPI initialization may be locking the system early
I would appreciate any guidance on hardware recovery steps, forced boot modes, or debugger connection techniques specific to STM32H7S7.
Thank you in advance.