USB-C Connector for Power Delivery and communication with STM32F767ZIT6
Hi
Here is my scenario:
I want to use USB Type C Connector for Power Delivery(upto 65W) and also, for communicating with STM32F767ZIT6 on my Hardware.
Power Delivery is used to charge a 14.4V Li Ion Battery using Battery charger on my hardware. So,
And USB Communication takes place with STM32F767ZIT6 Full Speed. Charging and Communication don't need to happen at the same time.
So, USB-C Connector will either be used to charge the battery using a AC-DC wall adapter or communicate with STM32 on my hardware using a USB-C Cable from PC. Only one of these things will happen at a time.
I was thinking of using STUSB4500 for Power Delivery such that it negotiates 20V, 3.25A with Wall Adapter but it looks like VBUS Sensing PA9 would be a problem when PC is connected(VBUS= 5V) or wall adapter is connected(VBUS= 20V).
So, wondering if there are better/easier options to do this? Changing the STM32F767ZIT6 to something like STM32 UCPD MCUs is unfortunately not an option.