Skip to main content
HNguy.25
Associate III
November 16, 2022
Solved

Variable runover before it reaches its limit

  • November 16, 2022
  • 2 replies
  • 2024 views

Hello everyone,

My variable had a Runover even before it reached its range.

Currently, I am working with timer 2 with a frequency of 90MHz. When I retrieved the current time by `__HAL_TIM_GET_COUNTER()` and printed it by `printf("receive_time: %lu\n", (unsigned long)receive_time)`, the maximum the `receive_time` get is 16 bits although I declared it as 32 bits. I observed the printed value and it never exceeded 2^16 -1. 

I also tried to print with `printf("%" PRIu32 "\n",a);` but it also returned the same. 

I had another 32-bit variable `send_time` which is used later to subtract with `receive_time`. However, it gave me something in the order of 2*10^9 (2147482170 for example) besides some common values.

I want to ask what happen and if I do something wrong. If everything is correct, is there any way to handle the rollover besides having 2 timers starting at different times?

The code is here:

Radio::radio.tx_buf[0] = seq++; /* set payload */
 
 printf("send a ready message\r\n");
 
 Radio::Send(1, 0, 0, 0); /* begin transmission */
 
 send_time = __HAL_TIM_GET_COUNTER(&htim2);
 
.
 
.
 
.
 
if (Radio::radio.rx_buf[0] == 100)
 
 {
 
 receive_time = __HAL_TIM_GET_COUNTER(&htim2);
 
 printf("receive_time: %lu\n", (unsigned long)receive_time);
 
 printf("send_time: %lu\n", (unsigned long)send_time);
 
 time_difference = (receive_time - send_time)/2;
 
 printf("time_difference: %lu\n", (unsigned long)time_difference);
 
 uint32_t distance = time_difference * 10 / 3;
 
 printf("Distance: %lu\n", (unsigned long)distance);
 
 }

Thank you in advance,

Huy Nguyen.

This topic has been closed for replies.
Best answer by Danish1

Sorry I was wrong about the 32-bit timer. I didn't spot you specifying which stm32 you were using, and many are only 16-bit even for TIM2.

Looking at e.g. stm32f4xx_hal_tim.h, I see __HAL_TIM_GET_COUNTER expands to

((__HANDLE__)->Instance->CNT)

It might be worth looking at the code your compiler generates, to verify that it is doing a 32-bit access to htim2.Instance->CNT

And with a debugger seeing if the top 16-bits in TIM2->CNT ever get set.

How strongly do you know that htim2 refers to TIM2?

Regards,

Danish

2 replies

Danish1
Lead III
November 17, 2022

The problem isn’t your variable.

The underlying hardware of stm32 timers is generally 16-bit. Have a look at the TIM section of the Reference Manual for your stm32 for a better understanding of the issues involved.

I strongly dislike ST’s HAL library because the documentation is inadequate. Although it helps users avoid “gotchas�?, users still need to understand the limitations of the underlying hardware, which is ONLY covered by the Reference Manual, Data Sheet and Programming Manual.

Hope this helps,

Danish

HNguy.25
HNguy.25Author
Associate III
November 17, 2022

Hello @Danish​ 

Thank you for your response. Before using the timer 2, I did check the manual about timer in the datasheet as below:

0693W00000WId0JQAT.pngAnd timer 2 has a counter of 32-bit.

That is why I got confused a bit.​

Danish1
Danish1Best answer
Lead III
November 17, 2022

Sorry I was wrong about the 32-bit timer. I didn't spot you specifying which stm32 you were using, and many are only 16-bit even for TIM2.

Looking at e.g. stm32f4xx_hal_tim.h, I see __HAL_TIM_GET_COUNTER expands to

((__HANDLE__)->Instance->CNT)

It might be worth looking at the code your compiler generates, to verify that it is doing a 32-bit access to htim2.Instance->CNT

And with a debugger seeing if the top 16-bits in TIM2->CNT ever get set.

How strongly do you know that htim2 refers to TIM2?

Regards,

Danish

HNguy.25
HNguy.25Author
Associate III
November 17, 2022

For the question "How strongly do you know that htim2 refers to TIM2?": it is in the initialization of timer 2. htim2 is just a name. And in the initialization function, the instance of htim2 is TIM2 (htim2.Instance = TIM2;)

As for your other suggestion, I will bear that in mind and check it. I think it is also about the maximum counter or Auto Reload Register (ARR).

I will update more.