WeAct BlackPill: Ocasional DFU problems in STM32CubeProgrammer on Windows 10
Hi Everyone,
I have some problems with DFU on Windows 10. I use WeAct BlackPill boards based on STM32F411 MCU. This board has BOOT0 button which allow to update firmware using STM32CubeProgrammer and DFU mode.
Majority of the boards can be programmed in DFU mode using STM32CubeProgrammer with no issue. Recently I got couple boards that acts very weird: those boards enters DFU mode just fine, detects by STM32CubeProgrammer and able to connect, but as soon I try to erase or program those boards - STM32CubeProgrammer says "Connection lost" and that is it. After that those boards enters into DFU mode, STM32CubeProgrammer able to read serial number, but any attempt to connect failed:
16:51:36 : STM32CubeProgrammer API v2.18.0 | Windows-64Bits
16:51:45 : UR connection mode is defined with the HWrst reset mode
16:51:45 : USB speed : Full Speed (12MBit/s)
16:51:45 : Manuf. ID : STMicroelectronics
16:51:45 : Product ID : STM32 BOOTLOADER
16:51:45 : SN : 337F33963134
16:51:45 : DFU protocol: 1.1
16:51:45 : Board : --
16:51:45 : Device ID : 0x0431
16:51:45 : UPLOADING OPTION BYTES DATA ...
16:51:45 : Bank : 0x00
16:51:45 : Address : 0x1fffc000
16:51:45 : Size : 16 Bytes
16:51:45 : UPLOADING ...
16:51:45 : Size : 1024 Bytes
16:51:45 : Address : 0x8000000
16:51:45 : Read progress:
16:51:45 : Error: Data read failed
16:51:45 : Warning: Connection to device 0x431 is lost
16:51:51 : Warning: Connection to device 0x431 is lost
16:52:00 : Disconnected from device.
16:52:00 : Disconnected from device.
If I use ST-Link to program those boards, I able to connect in DFU mode again... until I try to reprogram it. Then same problem with connection appears again.
I tried two different cables and three different laptops - same result.
But then I decided to try another PC with Windows 11 and it works! It works every single time on two different Windows 11 based laptops with no problems! STM32CubeProgrammer version is the same(2.18), so it is not that, it is something else. I wondering what it can be.
I really want this issue to be fixed, because I can't use those boards for my SmartPendant project to control CNC machines based on grblHAL controllers, since it will be impossible to update firmware under Windows 10, and even worse - attempt bricks device until it will be reprogrammed on Windows 11.


@Pavel A. wrote:> since it will be impossible to update firmware under Windows 10
Windows 11 works better than Win10. Sometimes newer is better. Support of Windows 10 will end in October anyway. Time to update!
I wondering why some people give advices that doesn't helps at all.Не зря СССР называли "страна советов"...
I make those devices and sell them to hobbyists like me who converting benchtop mills/lathes into CNC. They can use different OS and I have no control of it. I couldn't just say "Oh, you have a problem? Time to update!". Beside, I tried it on Windows. Will it have same problem on MacOS? On a Linux? I don't know. But what I do know there some problems with some of MCU, because some boards work and some don't. And those problems potentially can be fixed on STM32CubeProgrammer side since it works flawlessly on Windows 11.
And questions I want to be answered:
1) If it bug in MCU, does it affect anything beside DFU? Crushing CNC machine is not fun.
2) Will it be fixed in STM32CubeProgrammer?
P.S. I reposted it from there: https://community.st.com/t5/stm32-mcus-embedded-software/ocasional-dfu-problems-in-stm32cubeprogrammer-on-windows-10/m-p/765994/
since this is more appropriate section. You can delete original topic. <-- Threads merged