Why is any debug attempt on the STMF3348 discovery board always ending up in the hardware fault handler?
I am new to STM32 development and I have INCREDIBLE difficulties getting any example to run on any platform. I used to be able to run some very simple examples and even successfully implement changes on a TouchGFX-generated project, but changing the .ioc file was discouraged and quickly messed up things. More recently I have never managed to debug anything on the STMF3348 discovery board, let alone implement a DAC output (triggered from the timer and fed from DMA). If I am lucky if I reach the clock setup before falling over. Now, I have installed a cube F3 patch but none of the examples are visible, probably due to their different format (none was made for STM32CubeIDE but for SW4STM32 instead) and they do not show up in the MX tool. Anyhow, copying over the SystemClock_Config() did not help as the system fell over evern before the HAL_INIT() ?! There must be a problem with the hardware setup but the board selection should take care of that. Is that board somehow obsolete? Could it be the debug settings? (Connect under reset?). I have previously developed using ATMEL (Atmel Studio, Visual Code with Platform IO), and Analog Devices / TI (using IAR) and never experienced such issues.