X-CUBE-EEPROM software package fills up emulated EEPROM with zeros on every call to EE_Init()
I am using an STM32L422RB and I have added the X-Cube-EEPROM SW package (version 3.0.0). After intensive use I noticed that the eEEPROM driver is actually writing 64 bits of 0's to my emulated EEPROM space on every device power up or wakeup.
On further investigation this is linked to the function EE_Init which calls the function VerifyPagesFullWriteVariable(0U, 0U) and according to the code comments performs a dummy write of 0 to get rid of potential instability of line value 0x0xFFFFFFFF consecutive to a reset during write here.
Why is this done and can this behaviour be avoided as this is effectively wearing out the flash needlessly, my application needs to go in and out of Standby regularly to save power and these writes will create non-negligible Flash wear.
Related to this question.