Skip to main content
AKerm.1
Visitor II
October 12, 2024
Question

AC?DC conversion system

  • October 12, 2024
  • 1 reply
  • 520 views

Dear all

I would like design a circuit for AC/DC conversion of a 3 phase AC voltage with different frequency and different amplitude. The input power of the circuit can be changed form 4W up to 300W. Actually, circuit input is generated by a output of a 3 phase generator which is linked to a small wind turbine, so its frequency and output voltage varies considerably. Maximum output voltage is about 36v.

I appreciate it if you instruct me for using the ST parts (power modules) similar to VIPER31.

Best regards

Amin

1 reply

AScha.3
Super User
October 12, 2024
"If you feel a post has answered your question, please click ""Accept as Solution""."