Skip to main content
HKall.1
Associate
June 23, 2022
Solved

Can LED2472G be used as a shift register to drive signal relays?

  • June 23, 2022
  • 2 replies
  • 928 views

Can LED2472G be used as a shift register to drive signal relays with coil current of < 30mA. Can they be used as generic shift registers too?

Thanks!

Håvard.

This topic has been closed for replies.
Best answer by Peter BENSCH

Welcome, @Håvard Kalliainen​, to the community!

Well, LED2472G is a shift register, but it can only be used as such to a limited extent: the individual outputs (bits) are actually constant-current LED drivers, so they are not really suitable for logic purposes. But of course you can control the loads connected to the individual outputs logically in the same way as a shift register. Only the serial output is directly comparable with a classic shift register.

However, one could imagine using LED2472G to drive 30mA relays, even if this does not correspond to the original purpose. But you must not forget the usual free-wheeling diodes, which due to the unspecified avalanche energy should better be Schottky diodes, because only they are fast enough. Even ultra-fast diodes with a blocking time of 10...20ns are probably too slow not to damage the respective LED driver - at least nobody guarantees that.

Does it answer your question?

Regards

/Peter

2 replies

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
June 23, 2022

Welcome, @Håvard Kalliainen​, to the community!

Well, LED2472G is a shift register, but it can only be used as such to a limited extent: the individual outputs (bits) are actually constant-current LED drivers, so they are not really suitable for logic purposes. But of course you can control the loads connected to the individual outputs logically in the same way as a shift register. Only the serial output is directly comparable with a classic shift register.

However, one could imagine using LED2472G to drive 30mA relays, even if this does not correspond to the original purpose. But you must not forget the usual free-wheeling diodes, which due to the unspecified avalanche energy should better be Schottky diodes, because only they are fast enough. Even ultra-fast diodes with a blocking time of 10...20ns are probably too slow not to damage the respective LED driver - at least nobody guarantees that.

Does it answer your question?

Regards

/Peter

HKall.1
HKall.1Author
Associate
June 23, 2022

Yes, Thank you!

Håvard