Can T1635-600G replace T3035H-6G?
We selected the Triac ST# T1635-600G for refrigerator project, to control the compressor (inductive loads). Tested T1635-600G, the heat is very serious when passing 16A current, even using a heat sink temperature is more than 100°C. Therefore, I want to use T3035H-6G. May I ask how much heat sink is required for this model when it passes 16A? Or do you have app recommendations? Are there any guidelines on heat dissipation? Thank you!