Can the diode STPS2H100 used for freewheeling of inductive load ?
The datasheet suggest its suitable for SMPS / lighting power supplies. Not clear if they can be used for the inductive load at the output of the hotswap controller.
The datasheet suggest its suitable for SMPS / lighting power supplies. Not clear if they can be used for the inductive load at the output of the hotswap controller.
The DC fan then draws approx. 6A, so that the freewheeling diode must also be able to withstand at least this current, which is why a diode with higher current is recommended, e.g. the STPS10H100C.
Theoretically, you can also use a TVS, but with a 340W motor it is a challenge to find a suitable one. However, TVS in a suitable power class are typically significantly more expensive than a freewheeling diode as mentioned above.
It is also a question of the desired behaviour: with a freewheeling diode, the motor continues to run at falling speed, while the TVS limits the voltage and thus slows the motor down more.
Regards
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.