Skip to main content
Salman S
Visitor II
March 17, 2023
Question

Choosing a Transil for Triac Over voltage protection.

  • March 17, 2023
  • 0 replies
  • 756 views

Hi team,

I'm working on a 3 Phase (400Vrms) Power board control system. Regarding the over-voltage protection of the triac, AN1996 suggests to use Transil across Gate and A2 of the Triac. 

1) When Choosing a Transil, the peak voltage of our system is 565V. The maximum Vrm of the Transils available is 376V. Can I use two BZW06-342B in series which has Vrm of 342V each. So 342*2=684V will be the total Vrm. Will this work?

2) We have also planned to use MOV across the triac for additional Overvoltage protection. Could you please suggest us on the ratings of the varistor. Should it be below or above the Voltage ratings of the Transil.

This topic has been closed for replies.