Clarification in datasheet of VNL5300S5TR-E
I'm planning to use 24V 0.5A Motor in application. It will be controlled from MCU which is taking 3.3V input and it's GPIO will give 3.3V when output pin is logic high. I'm thinking to interface the Motor to MCU via driver VNL5300S5TR-E.
Now I have doubts in this driver VNL5300S5TR-E.
- This VNL5300S5TR-E IC is running on 3.5V to 5V. so I'm giving Vcc pin to 5V but input pin of this IC will be driven from MCU which will make input pin of IC to 3.3V.
so 3.3V voltage is sufficient to turn on the Internal MOSFET ?
2.There is a truth table 14 in the datasheet which says that STATUS Pin will get low for condition Output voltage < VOL. What is this condition, can you explain in detail.
3.Also what is this Openload detection table 10. in the datasheet. Can you tell more about this.
Regards,
Bitesh