Clarification on Maximum Voltage Limitation of EVLSTGAP3S6S Board
I am planning to purchase the EVLSTGAP3S6S evaluation board for my research. While reviewing the datasheet, I noticed that the board is specified to support a high-voltage rail of up to 520 V, limited by the MOSFETs and capacitors. However, I observed that:
- The board uses SCTH60N120G2-7 SiC MOSFETs, which are rated at 1200 V, 60 A.
- The film capacitor used (C4) is rated at 1.1 kV (Panasonic ECWFG1B335J).
Given that both components have voltage ratings above 1 kV, I would like to understand why the maximum voltage rail is limited to 520 V. I need to assess whether the board can support higher voltage operation (e.g., up to 800 V DC). Could anyone kindly clarify the reason for the 520 V limitation?